Browse FAQs



SurgeArrest - minimum install distance of 10 meters (30ft).
Do not install this device if there is not at least 10 meters (30 feet) or more of wire between the electrical outlet and the electrical service panel. ... The UL1449, 3rd Edition Standard is now broken out into "Type" designations ranging from Type 1- 5 . ... - Component Assemblies -,Component assembly consisting of one or more Type 5 components together with a disconnect (internal or external) or a means of complying with the limited current tests. ... Type 5
Video: What does the Site Wiring Fault Indicator LED on my APC UPS or Surge Arrestor represent?
... -UPS and SurgeArrest products ... -UPS and SurgeArrest products equipped with ... ... wire (> 5 Volts AC measured ... If the outlet that the APC UPS unit is plugged into is not properly grounded or properly wired, the unit will attempt to absorb the excess voltage instead of redirecting it to ground. ... Therefore, in order to maintain your warranty and protection under APC's Equipment Protection Policy, be sure that the APC unit is only plugged into a properly grounded outlet where the Site Wiring Fault Indicator (SWF) light is not illuminated.
Cable Picture Degradation When Using an APC Coaxial Surge Protector
SurgeArrest , Protectnet, Back-UPS, Back-UPS Pro, APC AV line of products ... It's insertion loss is at 1 GHz were attenuation is 5 dB. ... terminated cables from an electronics store ; such as Radio Shack. ... (available at many electronics stores ).
What are the operational conditions for an InRoom (Stulz) Unit
208- 230v / 3ph / 60 Hz ... Maximum level difference between the condenser and the cooling unit: 5 m (16 ft) when the condenser is below the cooling unit ... Humidity: (% R. H.): 5 - 95 ... Fluid outlet temperature (G): 40°C (104°F)
Why is the Protection Working LED of an APC SurgeArrest, or SurgeProtector off?
illuminate: 1. The unit is powered off (for 7 outlet SurgeArrest strips only).
Uniflair Pump Packages Technical Specs
ACPP2322 Dual Pump Package 5 HP 208- 230v /3/60 Hz
GFCI circuit breaker trips after UPS or SurgeArrest
Issue: GFI outlet , circuit breaker trips after UPS or SurgeArrest is connected.
Video: Data Center Expert | How do I control APC Switched Rack PDUs?
5 ) Select perform command and the commands will be issued to the outlets that are selected.
Is a service loop required on install of a TVSS SurgeArrest Panel Mount device?
Length of Free Conductors at Outlets , Junctions, and Switch Points. At least 6 in.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.