Browse FAQs



Can the horizontal cable troughs ar8008blk and ar8016ablk be used in conjunction with vertical cable managers ar7580a, AR7585 and AR7588?
... on the horizontal cable troughs will mount to ... rails when vertical cable managers ar7580a, ... ... cabinets, vertical cable management and horizontal troughs . All 750mm wide NetShelter SX ... ... -style vertical cable managers and horizontal cable troughs on the mounting rails of a 750mm wide NetShelter SX ... ... when using vertical cable managers such as ... still install the cable troughs which run front ... ... holes in the cable managers and prevent ... ... finger-style cable managers are a ... The center thru-hole in the mounting rails is covered by the AR7588.
Is there a depth extender for the rear or front of NetShelter SX cabinets? Is there a way to bay the rear of cabinets that are different depths?
The roof of the depth extender is not load bearing. Do not run cables , troughs or ladders atop the depth extenders.
Can I run cables over the SC? If so, how many?
Yes, there is a cable support bridge trough available as an accessory (acac10021).
How deep must the ar7580a Cable Manager be installed so the AR7581A Hinged Cover can open 90 degrees?
Cause: Customer needs to be able to fully open the hinged cable cover to add, move or change cables .
When finger-style vertical cable managers are used in a 750mm wide NetShelter cabinet, is it possible to also block off the cable pass-thru openings in the mounting rails?
When there are finger style cable managers installed inside the 750mm wide NetShelter cabinet, AR7714 must be used to prevent hot air recirculation.
Which NetShelter SX cabinet has a greater cable capacity, 750mm wide or 800mm wide?
Resolution: The 750mm wide and 800mm wide cabinets use the same vertical cable managers so they have the same cable management capacity.
What width cable ladder will attach to the pass-through data cable partitions?
NOTE: AR8164ABLK and AR8165ABLK both contain hardware that allow cable ladder to attach to the NetShelter partitions and troughs .
Uniflair BACnet (Building Automation and Control Networks)
All the units must be fitted with a RS485 card, trough that they are connected to the RS485 serial cable .
InRow RC Standard and Optional Features
Power Trough (Overhead power distribution between racks) Data Partion Trough (Allows removal of RC unit without disrupting cabling )


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.