Browse FAQs



Can the new NetShelter SX 12U and 18U cabinets be stacked?
Issue: A customer is asking if the new short NetShelter SX cabinets can be stacked.
Is there a depth extender for the rear or front of NetShelter SX cabinets? Is there a way to bay the rear of cabinets that are different depths?
The roof of the depth extender is not load bearing. Do not run cables, troughs or ladders atop the depth extenders.
Can the AR8125 NetShelter AV Sliding Shelf be installed into an SX cabinet?
... install the AR8125 NetShelter AV Sliding Shelf into an SX cabinet. NetShelter SX ... holes of the NetShelter AV cabinets. ... installed into an SX cabinet with square ... ... Will the AR8125 NetShelter AV Sliding Shelf Fit Into SX Cabinets? ... compatible to the SX series of cabinets ... In the NetShelter Compatibility Chart the ... ... mounted into an SX cabinet, or ... ... AR8125 into an SX cabinet? ... use with the NetShelter AV cabinets which ... ... 32 screws ( black in color) ... ... rails to the NetShelter AV’s #10 ... ... AR8125 to a NetShelter SX with square holed ...
Is it possible to convert a NetShelter SX Networking cabinet into a standard NetShelter SX cabinet?
You may leave it. If you want to replace it you'll find the NetShelter SX roofs in the NetShelter Compatibility Chart.
How many 0U accessory channels (RCC's) are included with NetShelter SX cabinets, and how manu PDUs can fit into them?
Resolution: All 1070 mm deep NetShelter SX cabinets have 2 0U accessory channels.
Are replacement parts available for my NetShelter SX ARU, ADU or Roof Fan?
Issue: There may be a need for NetShelter Roof Fan, ADU or ARU replacement parts.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.