Browse FAQs



What sensors are supported by the NetBotz Wireless Sensor Pod 180 (nbpd0180) ?
NetBotz Door Switch Sensor for APC Racks ... 12 ft nbes0303 NetBotz Door Switch Sensor for APC Racks ... 62 in nbes0313 NetBotz Door Switch Sensor for Third Party ... 62 in nbes0312 NetBotz Door Switch Sensor for Rooms or Third Part ... nbes0302 APC Temperature Sensor - 13 ft ... Temperature & Humidity Sensor - 13 ft ... the nbpd0180 AP9335TH NetBotz Temperature
Can I physically interconnect multiple NetBotz devices?
You should never try to interconnect multiple NetBotz appliances through USB ... to be used for sensor pod 150 or 155 units or an ap9520th.
Can I use a NetBotz Camera Pod 160 nbpd0160 / nbpd0160a as a standalone appliance?
... of using a NetBotz camera pod 160 on its ... NetBotz NetBotz The NetBotz Camera Pod 160 nbpd0160 / ... 570, or Room Monitor 455. The RJ45 connection that is on this camera pod is for the NetBotz door sensor . The camera can not be discovered by StruxureWare without a connection to a main NetBotz appliance. ... Purchase a Rack Monitor 450, 550, or 570, or Room Monitor 455 for functionality. If the camera is the nbpd0169a, please be sure you upgrade to version 4.6.2 or higher of the NetBotz Firmware (also known as BotzWare).
Version 2 NetBotz ​0-5V sensor on Sensor Pod 120 reports double the actual voltage in Advanced View
0-5V sensors connected to the NetBotz Sensor Pod 120 with the NetBotz 0-5V Sensor Cable (nbac0231) report ...
NetBotz | Can I change the address on a NetBotz A-link sensor pod or rack access pod?
NetBotz Appliances (200, 250, 355, 450, 455, 550, & 570) NetBotz Sensor Pods (nbpd0150 & nbpd0155)
NetBotz | Hardware & Software Support Information and Limits
... All attached downstream NetBotz Sensors and NetBotz Sensor Pods are covered under ... warranty of the NetBotz Appliance, except ... such as wireless sensor batteries (covered under Wireless Sensor factory warranty only ...
NetBotz 455 | Physical Description
3 A-Link port Used for cascading NetBotz sensor pods and temperature and humidity sensors with digital displays.
NetBotz 450/550/570 | Physical Description
13 A-Link port Used for cascading NetBotz sensor pods and temperature and humidity sensors with digital displays.
Can not configure events for NetBotz 200 external sensor pods.
Firmware limitation, sensor pod alarm configuration is not linked in UI.
Newer sensor pod 120 (nbpd0122) not appearing on older Netbotz V2 firmware.
Due to hardware and firmware changes on the newer Sensor pod 120, Botzware prior to ... is unable to properly detect the sensor pod .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.