acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... or XR Battery Cabinet is receiving input ... ... or XR Battery Cabinet , in case ... ... or XR Battery Cabinet . ... panels at the end of the row of the Hot ... Do not remove the rear doors of the UPS, PDU, or XR Battery Cabinet ... To attach the door frame to the end of the aisle: ... Install the side panels at the ends of each row of the Hot Aisle Containment System. ... Attach one end of a ground strap to the grounding stud on each panel, and then attach the other end of the grounding strap to a grounding stud on the enclosure.