Browse FAQs



APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units. Capacity KW ... W= Water Cooled ... F= Water Cooled ... D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled Capacity KW ... coil C= Chilled Water Capacity KW C= Chilled Water Capacity KW ... Main C= Chilled Water Capacity KW ... W= Water Cooled ... G= Glycol Cooled BA=208 ... Capacity KW ... W= Water Cooled ... G= Glycol Cooled 2 = 2 Bay 10 ( 2 Bay) 12 ( 2 Bay) 14 ( 2 Bay)
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... ELBOW 1/ 2 INCH - 15 ... ... STRAIGHT 1/ 2 INCH - 1/ 2 INCH PEX ( ... ... STRAIGHT 1/ 2 INCH - 15 ... ... - acrp1xx ( DX ... (CW AND DX ... FAN acrp1xx ( DX ) ... Reheat acrp1xx ( DX ) ... for acrp1xx ( DX ) ... /102 ( DX ) ... For acrp101 ( DX ) ... -240v # 2 0w3125 Cable Main ... -480v # 2 0w3126 CABLE TIE ... for acrp100 ( DX ) ... for acrp101 ( DX ) Circuit Breaker 2 P 5A ... ... r0357 Circuit Breaker 2 P 5A ...
How to navigate through an Network Air FM unit display
... APC NetworkAIR FM DX Precision Air Conditioner ... DX ... Direct expansion ( DX ) coil ... —Economizer and DX coils ... MultiCool® ( chilled water) and DX coils ... , then the cooling setpoint is used ... ... 48) / 2 = 0. ... ... the NetworkAIR FM DX 60 Hz ... avoid over- cooling while dehumidifying. ... the modes ( cooling , reheat, ... ... compressor (stage 2 ) in a ... ... the NetworkAIR FM DX 60 Hz Installation ... the NetworkAIR FM DX . ... for fluid- cooled options ... of fluid- cooled option. ... will switch the cool or dehumidify mode ...
Spare parts list for ACRD1XX, and ACRD2XX
... 0.079 110 .0 110 .0 110 .0 0 ... ... DOOR ASSY 10 KW - SPARE PART ... 195.0 2 ,000. ... ... 5.450 69 .0 1 ... ... CRAC 8X 2 FORM-C ... 2 .505 210 ... ... 0.071 110 .0 110 .0 110 . ... 50.0 110 .0 110 .0 W234 ... DP 2 POLE 30a 208 ... 0.293 110 .0 110 .0 110 .0 0 ... ... 0.315 110 .0 110 .0 110 .0 0 ...
Can you interconnect A-Links CW and DX InRow Cooling products?
B) acrc1xx +acrc5xx on the same A-Link 2 ) Can
NetBotz version 3.3 sensors do not update to modbus registers to double registers automatically upon upgrade.
For numbers greater than that, NetBotz appliances now allow for the use of 2 registers to monitor a single sensor.
How to read a pressure temperature chart for super-heat and sub-cooling calculations
... and sub- cooling calculations. All DX Cooling units. ... to Use a Two -Column Pressure ... ... to read a two -column PT ... ... (see Figure 2 ) ... zeotropic blends list two columns next to ... ... by 1 or 2 psi. ... small between the two values some manufacturers ... ... higher glide ( greater than 5° ... Using a two -column PT chart ... The problem with two -column PT charts is that the conditions a t the endpoints of the temperature glide are listed, not the midpoint. ... Two -column PT charts are every bit as useful as the traditional ones.
Where are your NetworkAIR FM DX manuals?
Where are your NetworkAIR FM DX manuals? ... Data Center Cooling ... The NetworkAIR FM DX has been discontinued and is not featured on our website as a current product. ... If you require more assistance, please call our technical support office at 888-695-6500 and hit option 2 three times. ... The modular, Floor Mount computer room air-conditioning system offers efficient, effective and economical cooling for a variety of spaces.
What are the minimum load requirements for the ACRP DX?
... for the ACRP DX ? InRow Cooling ... continually adjusts its cooling output to accommodate ... The cooling output is determined ... each of the cooling units in the cooling group if more than one cooling unit is present ... Fully loaded, the nominal cooling capacity of the equipment is 29 kW . At its lowest speed, the equipment cooling capacity is approximately 10 kW but is is recommended to have at least 13 to 15 KW of load per unit. Great consideration should be given to the loaded and unloaded state of the compressor to ensure that the operational range stays within these limits.
How do I update the firmware of my SRT series Smart-UPS using the Firmware Upgrade Wizard?
Devices that are *NOT* supported by the Firmware Upgrade Wizard: ... for the Firmware Upgrade Wizard are as ... ... 6KVA (firmware greater than 2. ... Upgrading SRT 5/ ... units from version 2 .x requires ... ... through the firmware upgrade process twice. The first upgrade will bring you ... and the second upgrade will bring you ... ... If you are upgrading an SRT unit ... have your external battery packs connected when you perform the upgrade . ... Upgrading an SRT unit may take up to 20 minutes to complete. ... The more external battery packs are connected, the longer the upgrade will take. ... If upgrading via USB, it is recommended that you use the included USB cable.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.