Browse FAQs



Schneider Electric's Technical Support Policy for Older Versions of PowerChute Software
... far beyond this stated commitment, but this 1 - year policy is stated here so customers may take it into account for planning purposes ...
Single Phase Symmetra Extended Run (XR) Frame Cable Lengths
This information can be relevant if a user is planning on installing the products in slightly different areas - different racks, for example.
Steps to take when moving a Symmetra Power Array from one location to another
... case you need to either send any components back to the APC or if you plan on moving your UPS in the future.
3 Phase Products Service Level Agreements; Definition of coverage as relates to the service level agreements offered by SE
UPS & PDU Advantage Plus: See attached file; ARUO-ACQK4F_R7_EN_ Advantage Plus ... 1 Annual PM Visit ... UPS & PDU Advantage Prime : See attached file; ARUO-ACQGSD_R7_EN_ Advantage Prime ... 1 Annual Preventive Maintenance Visit ... UPS & PDU Advantage Ultra: See attached file; ARUO-ACQFVH_R6_EN_ Advantage Ultra ... 1 Annual Preventive Maintenance Visit 1 Set of air filters if applicable
Problem: PowerChute Network Shutdown does not turn off the UPS following a shutdown event.
... of the PowerChute service , e. ... To make sure the UPS turns off as planned when a shutdown event occurs, PowerChute shutdown events should be configured with a delay of 120 seconds. ... This issue also applies to the Advanced Configuration option in Multiple Mode which, in a Multiple configuration, enables you to turn off one UPS when it goes on battery.
Rack PDU 2G (AP8XXX) Network Port Sharing Information
... ability to share one IP address via one network connection) ... PDUs using only one ... a number, 1 to 4, ... ... are connected to one another in a ... ... Sharing groups you plan to have. ... " port of one of the grouped ... ... desired order, 1 to 4. ... ... have Display ID 1 . ... access to outlets 1 , 2, ... 3 on unit 1 , ... 2, outlets 1 through 6 ... , and outlets 1 ,2, ... APC- Service -Type = ...
What are the typical uses for an EcoAisle System
Capacity Planning ... 1 U Servers
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... ... who uses any one of the products ... One such example is ... ... future firmware update plans to address this ... ... Network Management Card 1 (NMC1) ... a value of 1 to allow fallback ... Network Management Card 1 (NMC1) Information Bulletin: Effects of Microsoft Internet Explorer and other web browsers blocking key lengths less than 1024 bits​(blocking key lengths less than 1024 bits)
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
1 . Never work ... IF you plan to install a ... 1 . Remove the ... 1 . Attach two ... 1 . Apply the ... 1 . Remove the adhesive backing film from the panel frame; remove the protective plastic from both sides of the Lexan and carefully set the Lexan panel in place, pressing the edges firmly. ... 1 . Attach the door frame assembly to the equipment frames. ... Attach one end of a ground strap to the grounding stud on each panel, and then attach the other end of the grounding strap to a grounding stud on the enclosure.
What are the Dynamic Load ratings and Shipping Load ratings for NetShelter CX cabinets?
Persons planning data centers need to know how much weight can be loaded into the NetShelter CX for static installation, dynamic installation (rolling on flat surface) or to ship loaded with equipment. ... This is the maximum allowable weight of equipment installed in the cabinet during movement from one location to another within the same data center. ... Example: a customer who wishes to move a cabinet from one row to another in a data center must remove equipment until the weight is equal to (or below) the Dynamic Load Rating before being moved.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.