Smart-UPS VT-Galaxy 3500; Bypass Not Available Input Freq/Volt Out Of Range, Output: Inverter sync. to bypass alarms
Smart- UPS VT- Galaxy 3500; Bypass ... Smart- UPS VT- Galaxy 3500-ais3000 ... occurs when the UPS is online, ... , the UPS should not allow ... to command the UPS to bypass. If the UPS allows you to ... ... window, the UPS should be in ... For 60 Hz systems: 60 HZ +/- 0, 1 % ... 50 Hz - 70 Hz For 50 Hz systems: 50 HZ +/- 0, 1 % ... 40 Hz - 60 Hz ... When AC mains returns you may get a informational event for; Mains no longer prevents UPS from switching to bypass.