Browse FAQs

PowerChute Network Shutdown – Hosts fail to enter maintenance mode when vSphere Clustering Service (vCLS) is enabled

Published date: 05 February 2021

Issue:
PowerChute Network Shutdown – vSphere Clustering Service (vCLS) introduced in VMware vSphere 7.0 update 1 prevents hosts from entering maintenance mode since vCLS agent VMs cannot be shut down


Products:
PowerChute Network Shutdown v4.x

Environment:
VMware vSphere 7.0 update 1

vCenter Server Appliance 7.0 update 1

Cause:
vSphere 7.0.1 introduced a new feature called vSphere Cluster Services (vCLS) that allows DRS and HA to continue functioning even when vCenter Server is unavailable.


The issue occurs because there are 3 vCLS Agent VMs deployed in the cluster that cannot be powered off during the VM Shutdown step along with other User VMs. When vCenter Server detects that these VMs are powered off, it will automatically power them back on. Since these VMs remain powered on, the Hosts on which they reside cannot be placed into maintenance mode.

Solution:
Enable VM Prioritization and add all User VMs to a priority group except for the vCLS VMs. vCLS VMs are named vCLS (<number>).

Configure a 0 second duration for VM Shutdown and VM Startup for the Un-prioritized group. This ensures that the vCLS VMs will not be shut down or powered on by PowerChute.

Ensure that Delay Maintenance Mode is enabled.

Please follow the instructions in the attached PDF (vCLS_ScriptInstructions). Alternatively, if you are not using DRS, you can choose to disable vCLS permanently by following the instructions here - https://kb.vmware.com/s/article/80472
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.