Technical FAQs

Ask a Question

Is there a height difference between NetShelter cabinets with standard castors and heavy duty castors?

Issue:
A customer is asking about height difference caused by changing the castors. 

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
There may be a height difference when the castors are changed. 

Resolution:

There is no height difference on a cabinet if it uses standard castors or heavy duty castors. This includes AR3xxx, AR3xxx-717, AR3xxxSP. 
Was this helpful?
What can we do to improve the information ?