Technical FAQs

Ask a Question

What is the distance between PDU mounting holes on the NetShelter SX accessory rails?

Issue:


Product Line:


Environment:
All versions and serial ranges.

Cause:


Resolution:

In the 42U cabinet 
There are 6 sets of PDU mounting holes, all are spread by 7U (311mm 12.25") 

In the 45U cabinet 
There are 6 sets of PDU mounting holes, all are spread by 7U (311mm 12.25") 

In the 48U cabinet 
There are 6 sets of PDU mounting holes, all are spread by 7U (311mm 12.25") 
Was this helpful?
What can we do to improve the information ?