Technical FAQs

Ask a Question

Which NetShelter SX cabinet has a greater cable capacity, 750mm wide or 800mm wide?

Issue:
A customer asks if the 800mm wide NetShelter cabinet has a larger cable management capacity. 

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
A customer is trying to choose 750mm vs. 800mm wide cabinets. 

Resolution:

The 750mm wide and 800mm wide cabinets use the same vertical cable managers so they have the same cable management capacity. 
For example; AR7580A is the high volume vertical cable manager used in AR3150 and AR3350, and also in AR3180G and AR3380G. 
Was this helpful?
What can we do to improve the information ?