Technical FAQs

Ask a Question

Heatcraft Condenser Sound Data

Issue:
Heatcraft Condenser Sound Data

Product line: 
Heatcraft Larkin LNH Condenser

Environment:    

Cause:   
Heatcraft Condenser Sound Data

Resolution:  
See Charts below for sound data on a Heatcraft LNH condenser. 
Note Condensers require adequate spacing and placement away from structures to avoid sound attenuation. Some models offer a low noise theshold for residential applications.  These typically consist of lower RPM fans and a modified fan blade.

 

Was this helpful?
What can we do to improve the information ?