Technical FAQs

Ask a Question

There are different types of NetBotz Sensor Extender Cables, this article explains what the differences are.

Issue:

There are different types of NetBotz Sensor Extender Cables, this article explains what the differences are.

Product Line:

NetBotz

Environment:

NetBotz Cables.

Cause:

sensor options

Resolution:

We offer 2 different types of cables
1. Low Smoke Zero Halogen
2. Plenum rated cables are slow-burning, have fire-resistant casing and emit little smoke
 
Was this helpful?
What can we do to improve the information ?