Technical FAQs

Ask a Question

What are the pinouts for the Output Relay on the Environmental Monitoring Unit (AP9319) and the Environmental Management System (AP9320)?



Below are the pinouts:


 

Pin #

 Description

 1

 No Connection

 2, 3

 Normally Closed (NC) Contact

 4, 5

 Common

 6, 7

 Normally Open (NO) Contact (recommended connection)

 8

 No Connection


Relay ratings: 1A, 30V AC/DC



Since the user interface allows for either 'normally open' or 'normally closed,' APC recommends using only the normally open contacts and configuring the 'normal' state in the user interface.



 

Was this helpful?
What can we do to improve the information ?