Technical FAQs

Ask a Question

RS-485 Converters for the UPS SmartSlot Building Management Card (AP9622)



Issue

RS-485 Converter Compatibility for AP9622 Building Management Modbus/JBUS UPS SmartSlot card


Product Line
  • UPS Device Management
    • AP9622 Building Management Modbus/JBUS UPS SmartSlot Card 


Environment

AP9622 installations requiring RS-232 to RS-485 converter to work with various Building Management Systems


Cause

The AP9622 card supports RS-232 Modbus/JBUS output. Users may require RS-485 adapters to work with an existing Building Management System. Refer to compatibility list below.


Resolution


The Building Management Integration Card (AP9622) will work with the following RS-232 to RS-485 converters:
  • B&B Electronics P/N: 485OT9L*
*Item is currently discontinued per B&B. The recommended replacement is 4WSD9OTB but it has not been tested with the AP9622.
 
  • B&B Electronics P/N: 485LP9TB 
Below is an example diagram for a 485LP9TB application:

 

 
Was this helpful?
What can we do to improve the information ?