TradeOff Tools

:
-or-
:

ATTENTION: For instructions on how to properly link to these TradeOff Tools, click here 5 result(s) found.
Number Title & Description
TT-0 v0 Rack Power Architecture Efficiency Calculator
Compare conventional to 12V to 48V PSU & VRM architectures
TT-0 v0 Temperature Rise after Power Loss Calculator
Mitigate temperature rise when power and cooling is lost
TT-0 v0 IT Pod Sizing Calculator
Determine electrical & physical attributes of a pod based on input voltage, input breaker size, and rack density
TT-0 v0 PRESENTATION: TradeOff Tools Overview
This presentation provides an introduction to APCs TradeOff Tools and describes each of the tools currently available.
TT-0 v0 Three Phase UPS Modernization Opex Calculator
Estimate the opex savings of replacing an aging 3-phase UPS with a new UPS