Browse FAQs

How to Add a power cable to the InfraStruXure PDU(PDRPPH1000) ?

Published date: 08 July 2020

Add a power cable to the PDU :

Before adding a power cable, add a circuit breaker:
1. Install a strain-relief connector in
any available knockout on the roof
of the PDU.
2. Slide enough of the power cable
through the strain-relief connector to
reach the new circuit breaker.
3. Tighten the strain-relief connector.
4. At the front of the PDU, connect the power cordís individual wires:
a. If you have branch current monitoring installed, route the phase conductor through a current
sensor.
b. Connect the line wire to the circuit breaker.
c. Connect the neutral wire to the closest open termination point on the Neutral Bar (N).
d. Connect the PE wire to the closest open termination point on the PE Bar (PE).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.