Browse FAQs

How to Add a power cable to the InfraStruXure PDU(PD60H5HK1) ?

Published date: 08 July 2020

Add a power cable to the PDU :

Before adding a power cable, add a circuit breaker:
1. Install a strain-relief connector in any available knockout on the roof of the PDU.
2. Slide enough of the power cable through the strain-relief connector to reach the new circuit breaker.
3. Tighten the strain-relief connector.
4. At the front of the PDU, connect the power cordís individual wires:-
  •  If you have branch current monitoring installed, route the phase conductor through a current sensor.
  •  Connect the line wire to the circuit breaker.
  •  Connect the neutral wire to the closest open termination point on the Neutral Bar (N).
  •  Connect the PE wire to the closest open termination point on the PE Bar (PE).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.