Browse FAQs

How to Control console in InfraStruXure PDU(PD60H5HK1) ?

Published date: 08 July 2020

Control console :

After you log on at the control console.

1. Choose Network from the Control Console menu.
2. Choose TCP/IP from the Network menu.
3. If you are not using a BOOTP or DHCP server to configure the
TCP/IP settings, select the Boot Mode menu. Select Manual boot mode, and then press ESC to
return to the TCP/IP menu. (Changes will take effect when you log out.)
4. Set the System IP, Subnet Mask, and Default Gateway address values.
5. Press CTRL-C to exit to the Control Console menu.
6. Log out (option 4 in the Control Console menu).

Note : If you disconnected a cable during the procedure, reconnect that cable and restart the associated service.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.