Browse FAQs



How to connect 12 V external batteries with br1000guxi ?
1 . Remove the safety covers on the battery terminals. 2. Use the short jumper cable to connect the negative terminal on battery 1 to the ... 3. Locate the color coded cable with the 3 pin cable assembly . Connect the red cable to the positive terminal on battery 1 . ... Connect the 3 pin connector to the external battery receptacle on the rear panel
How to connect 12 V external batteries with br1500guxi ?
1 . Remove the safety covers on the battery terminals. 2. Use the short jumper cable to connect the negative terminal on battery 1 to the ... 3. Locate the color coded cable with the 3 pin cable assembly . Connect the red cable to the positive terminal on battery 1 . ... Connect the 3 pin connector to the external battery receptacle on the rear panel
How to Apply Power to PDU (pdrpph1000)?
1 . Close (turn ON) the main circuit breaker of the power source supplying power to the PDU. ... 3. Power the PDU distribution circuit breakers. ... Note: After the Main Output circuit breaker has been closed, both PDU distribution panels will be ... b. Close (turn ON) the PDU distribution panel circuit breakers. Note : When the distribution panel circuit breakers are closed, the PDU power cables
How to Apply Power to PDU (pd60h5hk1)?
1 . Close (turn ON) the main circuit breaker of the power source supplying power to the PDU. ... 3. Power the PDU distribution circuit breakers. ... Note: After the Main Output circuit breaker has been closed, both PDU distribution panels will be ... b. Close (turn ON) the PDU distribution panel circuit breakers. Note: When the distribution panel circuit breakers are closed, the PDU power cables
Video: Data Center Expert | Backing up to a Windows Share
1 ) Create a ... 1 ) Open the ... ... do not overwrite one another and a ... ... to the current allocation should more space ... ... share as a remote repository. Data Center Expert does not currently support version of SMB higher than version 1 . We are aware of the need to support higher version(s) of SMB and are working on upgrading the Operating System that Data Center Expert uses. ... Microsoft began disabling SMB version 1 in Windows Updates.
How to Install Hardwire PDU (ap7520) with any UPS ?
configuration. 4. Replace and secure the cover removed in step 1 .
Using Zentyal Linux FreeRADIUS along with APC Network Management Card Devices
: Go to the Configuration->Security-> Remote Users->RADIUS and modify one of the default server configurations.
How to add a circuit breaker on the InfraStruXure PDU(pd60h5hk1) ?
2. Snap the new single -pole circuit breaker into a position on the panel .
How to add a circuit breaker on the InfraStruXure PDU(pdrpph1000) ?
2. Snap the new single -pole circuit breaker into a position on the panel .
MAC address Vendor ID of Network Management Cards, and other network devices changing
A MAC address is a unique identifier given to a network card when it is manufactured .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.