Browse FAQs



How to Add a power cable to the InfraStruXure PDU(pd60h5hk1) ?
Add a power cable to the PDU : Before adding a power cable , add a circuit breaker: 1 . Install a strain-relief connector in any available knockout on the roof of the PDU. 2. Slide enough of the power cable through the strain-relief connector to reach the new circuit breaker. 3 . Tighten the strain-relief connector. ... Connect the neutral wire to the closest open termination point on the Neutral Bar (N). Connect the PE wire to the closest open termination point on the PE Bar (PE).
How to Add a power cable to the InfraStruXure PDU(pdrpph1000) ?
Add a power cable to the PDU : Before adding a power cable , add a circuit breaker: 1 . Install a strain-relief connector in ... 2. Slide enough of the power cable ... 3 . Tighten the strain-relief connector. ... c. Connect the neutral wire to the closest open termination point on the Neutral Bar (N). d. Connect the PE wire to the closest open termination point on the PE Bar (PE).
How to Apply Power to PDU (pdrpph1000)?
... below steps to Apply Power to PDU ... 1 . Close (turn ON ... 2. Close (turn ON) the Main Input on the PDU. 3 . Power the PDU distribution circuit breakers. ... a. Close (turn ON) the Main Output circuit breaker on the PDU. Note: After the Main Output circuit breaker has been closed , both PDU distribution panels will be ... b. Close (turn ON) the PDU distribution panel circuit breakers. Note : When the distribution panel circuit breakers are closed , the PDU power cables
How to Apply Power to PDU (pd60h5hk1)?
... below steps to Apply Power to PDU ... 1 . Close (turn ON ... 2. Close (turn ON) the Main Input on the PDU. 3 . Power the PDU distribution circuit breakers. ... a. Close (turn ON) the Main Output circuit breaker on the PDU. Note: After the Main Output circuit breaker has been closed , both PDU distribution panels will be ... b. Close (turn ON) the PDU distribution panel circuit breakers. Note: When the distribution panel circuit breakers are closed , the PDU power cables
How to connect contacts to the InfraStruXure PDU(pd60h5hk1) monitoring unit ?
1 . Choose one or more contact numbers on the user connection plate to which you will connect the ... f. Press the Down arrow key to enter a unique Name for the contact and to configure the ... Normal state of the contact (Open or Closed ). ... 3 . Connect contact wires (300v-rated cabling required) to the User Contacts terminal block on
How to connect contacts to the InfraStruXure PDU(pdrpph1000) monitoring unit ?
1 . Choose one or more contact numbers on the user connection plate to which you will connect the ... f. Press the Down arrow key to enter a unique Name for the contact and to configure the ... Normal state of the contact (Open or Closed ). ... 3 . Connect contact wires (300v-rated cabling required) to the User Contacts terminal block on
Video: Troubleshooting no communication between UPS and PowerChute Business Edition
1 . Once you have followed the steps outlined in the Troubleshooting sections above, stop and restart the PowerChute Business Edition Agent. If the system is still unable to communicate, proceed to the next step. 2. If you have a SmartSlot accessory connected to the UPS, check that it is configured correctly. More information regarding these accessories is available on 3 . If you still have not established communication, try using another communications (Serial/USB) cable if one is available. If you have tried all of the techniques above but have still not established communication, visit for troubleshooting help. 1. Make sure that the serial cable that came with the UPS is connected from the serial port on the UPS to the serial port on your computer. 2.
Network Management Card 3 - CDC-USB driver on Windows
Network Management Card 3 (ap9640, AP9641) ... Windows 7 operating systems connected to NMC via the USB serial console cable ... 1 . Connect USB ... 3 . User must choose to update their device driver and manually select the path to the .inf ... 1 . Connect USB ... 3 . Windows associates the device with the usbser.sys
How to Recover from a Lost Password in PDPM277H ?
1 . At the ... 2. Connect the provided serial cable to the computer and the port on the PDU. 3 . Run a terminal program (such as HyperTerminal®) and configure the port for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control. ... – The serial port is not in use by another application . – The terminal settings are correct as specified in step 3 . – The correct cable is being used as specified in step 2.
How to Recover from a Lost Password in PDPM144F ?
1 . At the ... 2. Connect the provided serial cable to the computer and the port on the PDU. 3 . Run a terminal program (such as HyperTerminal®) and configure the port for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control. ... – The serial port is not in use by another application . – The terminal settings are correct as specified in step 3 . – The correct cable is being used as specified in step 2.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.