Technical FAQs

Ask a Question

Video: How to verify USB communications between UPS and Windows OS using UsbDeview.exe
Issue: need to check USB communications between Windows OS and APC Back-UPS or APC Smart-UPS
What are the components required to install Power Chute Business Edition software?
... Agent can manage any UPS that is shipped ... , including most Smart-UPS ™ devices ( ... ) communicating using serial or USB connections.
How to Configure UPS connection settings using UPS terminal mode in Smart-UPS src1000iccind / src1000uxind ?
disconnect USB cable prior to connecting serial cable. 1. Open a terminal program, such as HyperTerminal
"How to Configure the number of battery strings using UPS terminal mode in Smart-UPS src1000iccind / src1000uxind ? "
disconnect USB cable prior to connecting serial cable. 1. Open a terminal program, such as HyperTerminal
What is the part number of APC Smart-UPS RT 15ft Extension Cable for 192VDC External Battery Packs ?
APC Smart-UPS RT 15ft Extension Cable for 192VDC External Battery Packs : surt008
Where can I get the Power Chute Business Edition sofware
You receive a PowerChute Business Edition CD in the box with your APC Smart-UPS (5kva & below).
What to do when the "Overload LED" on a Smart-UPS is illuminated?
Smart-UPS ... models, All Serial Numbers ... equipment from the UPS to eliminate the ... ... equipment from the UPS to eliminate the ... ... to trip the UPS circuit breaker, ... If the circuit breaker trips or the UPS attempts to transfer to battery in an overload condition, the load's power will be shut off. Turn the UPS off then back on to power the loads. ... If the Overload LED remains illuminated even without any load plugged into the UPS , the UPS has most likely sustained a surge or fault, and will need to be replaced. Contact APC Technical Support to resolve the problem.
How to Configure the number of battery strings using NMC terminal mode in Smart-UPS src1000iccind / src1000uxind ?
Connect the serial cable to the serial com port on rear side of UPS . ... Select the COM port that is connected to your UPS . ... 5. Press ENTER to initiate connection to UPS . ... – User Name: apc – Password: apc
Video: How do I configure APC Network Management Card network settings?
... Switches (AP44XX), Certain Audio/Video Network Management Enabled products, Smart-UPS Online (SRT).
Results 1 - 10 of 50