{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What do if UPS model SRV6KUXI-IN is not powering on ?

Probable cause:

1. The Easy-UPS is not turned on.
2. The Easy-UPS is not connected to the utility power supply.
3. Input circuit breaker on the Easy UPS is tripped.

Possible Solution:

1. Press the POWER ON/OFF button to turn on the Easy-UPS.
2. Check that the power cable from the Easy-UPS to the utility power supply is securely connected at both ends.
3. Turn on the circuit breaker in the rear panel.
In case if the issue persists even after trying the above troubleshooting, log the complaint.

Did this answer your question?

Explore more
Product:
SRV6KUXI-IN
Explore more
Product:
SRV6KUXI-IN
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.