{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What do if UPS model SRV6KUXI-IN is giving less back up?

Probable cause:

1.    Weak batteries.
2.    The Easy-UPS battery is discharged due to a recent power outage.
3.    The battery is near the end of its service life.

Possible Solution:

1. Check the load percentage via the display.
2. Frequent power failures would lead to low battery, ensure the batteries are allowed to charge completely after every discharge.
3. If the battery is near the end of its service life, consider replacing the battery, even if the replace battery indicator is not illuminated.
In case if the issue persists even after trying the above troubleshooting, log the complaint.

Did this answer your question?

Explore more
Product:
SRV6KUXI-IN
Explore more
Product:
SRV6KUXI-IN
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.