{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

LB1000UNO Luminous UPS is working on battery mode though utility/main supply is available

Probable cause:

1. Utility power is unavailable.
2. UPS input chord is not connected properly or partially connected to utility supply.
3. UPS is sensing Low or high input voltage to operate on mains.
4. Utility power is through incompatible source like extension or surge.

Possible solution:

1. Reconnect the power cord properly.
2. Do not use extension cord or surge suppresser at input of UPS.
3. Wait for the nominal utility supply.

In case if issue persist even after trying the above troubleshooting, log the complaint.

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
LB1000UNO
Explore more
Product:
LB1000UNO