{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Our Brands

{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

How many batteries can be connected to SRC3KUXI?

1. Connect six SMF/Flooded 12 V batteries in series. 
2. The UPS is intended for use with 72 VDC nominal battery voltage. The external battery system connected to the UPS must not exceed 72 VDC nominal voltage.
3. Multiple strings of each 72 VDC can be connected in parallel.

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.