{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
How many batteries can be connected to SRC1KUXI?
1. Connect two SMF/Flooded 12 V batteries in series.
2. The UPS is intended for use with 24 VDC nominal battery voltage. The external battery system connected to the UPS must not exceed 24 VDC nominal voltage.
3. Multiple strings of each 24 VDC can be connected in parallel.
2. The UPS is intended for use with 24 VDC nominal battery voltage. The external battery system connected to the UPS must not exceed 24 VDC nominal voltage.
3. Multiple strings of each 24 VDC can be connected in parallel.
Explore more
Product:
Explore more
Product:
Can't find what you are looking for?
Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.