Do we have "Mute" option available in APC make BVX900LI-IN Easy UPS?
Published date:
12 March 2021
Yes, there is an option to mute the audible alarm. Along with that, the Easy UPS is able to temporarily mute user correctable audible alarms such as On Battery, Overload and Low Battery status.
Note: Audible alarms for other critical events such as "Battery Replacement and Charger Notification" cannot be temporarily muted. The unit in these cases must be turned off.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.