What is the procedure to install Battery Connector in APC make BVX1200LI-IN Easy UPS?
Published date:
12 March 2021
Before performing the following steps, please ensure UPS is not connected to the power supply. Step 1. In UPS back panel, Pull the Battery Connector from its seating. Step 2. Rotate the Battery Connector clockwise. Step 3. Push the battery connector into the slot till it locks in position. Step 4. Make sure Battery Connector is properly placed in the slot.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.