Browse FAQs

Does APC make BVX1600LI-IN Easy UPS have "USB Charging Port"?

Published date: 12 March 2021

Yes, BVX1600LI-INEasy UPS has "USB Charging Port".
The USB charging port provides a maximum of 5 V / 2 A DC power. The port will charge the connected equipment when the Easy UPS output is on.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.