Browse FAQs

What to do if Replace battery LED illuminates in UPS SURT2000XLIM ?

Published date: 27 December 2019

Possible cause: 
a) Weak battery. 
b)Battery not connected properly. 
Solution:
1) Allow the battery to recharge for at least 24 hours. Then, perform a self-test. If the problem persists after recharging, replace the battery. 
2) Check that the battery connector is fully engaged. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.