What to do if Replace battery LED illuminates in UPS SURT1000XLIM ?
Published date:
27 December 2019
Possible cause: a) Weak battery. b)Battery not connected properly.
Solution:
1) Allow the battery to recharge for at least 24 hours. Then, perform a self-test. If the problem persists after recharging, replace the battery.
2) Check that the battery connector is fully engaged.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.