Browse FAQs

UPS SRC1KXLI is showing "SHORT" error on display with continuous alarm ?

Published date: 20 April 2020

Possible cause: UPS has experienced a short circuit at the output.Unit will try to auto recover from this condition.
Solution:1) Check if there is any short circuit at the UPS output.
2)Remove the short circuit. Wait for the unit to auto-recover or press POWER ON/OFF button to start the UPS.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.