Browse FAQs

UPS SRC1KXLI is not powering ON ?

Published date: 28 November 2019

Possible cause: 
a)The UPS is not turned on. 
b)The UPS is not connected to utility power supply. 
c)Input thermal circuit breaker on the UPS is tripped                                                                                                                                                                                                                                                                                                                     
Solution: 1)Press the POWER ON/OFF button to turn on the UPS.                                                                                                                                                                                                                                                     
2)Check that the power cable from the UPS to the utility power supply is securely connected at both ends.                                                                                                                                                           
3)Press the input thermal circuit breaker reset button in the rear panel.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.