What is Frequency converter mode and how to disable and enable mode in ups SRC1KXLI through display.
Published date:
28 November 2019
Kindly find the steps to configure output frequency for UPS SRC1KXLI.
Allows the user to set a constant output frequency of 50 Hz or 60 Hz
1. Press SELECT button to enter the UPS settings.
2. Navigate through the parameters using SELECT button.
3. Press ENTER/MUTE button to edit a Frequency converter mode. The icon starts flashing to indicate it is ready for editing.
4. Press ENTER/MUTE button to Select enable or disable option,the flashing of icon stops after the selection.
5.Select program00 to exit the navigation menu.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.