How to add a circuit breaker on the InfraStruXure PDU(PD60H5HK1) ?
Published date:
08 July 2020
Add a circuit breaker on the PDU :
1. Move the clip on the back of the circuit breaker to correspond to the phase to which you are connecting to (L1, L2, or L3).
2. Snap the new single-pole circuit breaker into a position on the panel.
3. Remove the corresponding plastic blanking plate on the front panel of the PDU.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.