Browse FAQs

How to add a circuit breaker on the InfraStruXure PDU(PDRPPH1000) ?

Published date: 08 July 2020

Add a circuit breaker on the PDU :

1. Move the clip on the back of the circuit breaker to correspond to the phase to which you are connecting to (L1, L2, or L3).
2. Snap the new single-pole circuit breaker into a position on the panel.
3. Remove the corresponding plastic blanking plate on the front panel of the PDU.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.