RX/TX (10/100) LED indication is Off in NMC card AP9635 ?
Published date:
05 July 2020
Probable cause:
• The NMC is not receiving input power.
• The cable that connects the NMC to the network is disconnected or not functioning properly.
• The device that connects the NMC to the network is turned off or not operatingcorrectly.
• The NMC itself is not operating properly.
Solution: It may need to be repaired or replaced.Contact APC by Schneider Electric Customer Support.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.