How to EDIT PORT NAMES in ADM submenu function for AP5202 model ?
Published date:
11 July 2020
Follow the below steps :
Assigns a unique name to each port to recognize a portís
corresponding computer. To create, modify, or delete port
names:
1. Click on or highlight a port using the navigation keys,
and press ENTER.
2. Type a new port name, or modify or delete an existing
name. The maximum number of characters allowed is
twelve, and the following characters are valid:
a Alphabetic: AñZ
b Numeric: 0ñ9
c Non-alphanumeric: +-/.%[ ] and Space
Port names are not case-sensitive and appear as all
capital letters regardless of how they were input.
3. When you are finished, press ENTER to save your
changes. Press ESC to cancel.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.