Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
Power Chute Business Edition agent is not working while the system is on stand by mode
The Power Chute Agent Windows service does not work while the computer is in Standby mode.
If your Windows computer is on standby at the time for which a shutdown is scheduled, the shutdown starts after standby mode ends. This is true even if the time scheduled for the shutdown (through the Shutdown Schedule command) has already passed.
If your Windows computer is on standby at the time for which a shutdown is scheduled, the shutdown starts after standby mode ends. This is true even if the time scheduled for the shutdown (through the Shutdown Schedule command) has already passed.
Did this answer your question?
Explore more
Explore more