Browse FAQs

What to do if my UPS SURT15KUXI is showing "UPS Is Overloaded"?

Published date: 09 June 2020

Kindly check the following condition if the SURT15KUXI is overloaded: 

1) Decrease the load
2) Check the load distribution on the three phases through the Power View display. 
3) If the load is unevenly distributed, adjust the load distribution.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.