Browse FAQs

How can we do Resetting the Network Interface in AP86** model ?

Published date: 03 June 2020

Path: Control > Network > Reset/Reboot
This menu gives you the option to reset and reboot various components of the network interface.
Users have the option to Reboot Management Interface,
Note: Rebooting the Management Interface only restarts the Rack PDU’s Network Management
Interface. It does not affect the outlet ON/OFF status.
Reset All: Clear the Exclude TCP/IP checkbox to reset all configuration values; mark the Exclude
TCP/IP checkbox to reset all values except TCP/IP.
Reset Only: (Resetting may take up to a minute) Options include:
• TCP/IP settings: Set TCP/IP Configuration to DHCP & BOOTP, its default setting,
request requiring that the Rack PDU receive its TCP/IP settings from a DHCP or BOOTP
server. See “View the result of the test DNS in the Last Query Response field.”
• Event configuration: Reset all changes to event configuration, by event and by group,
to their default settings.
• Guest PDU lost communication alarms by removing corresponding guest PDUs.
• Host Display ID and Remove all Guest PDUs.
• RPDU to Defaults.
• For NPS groups:
Guest PDU lost Communication alarms by removing corresponding guest PDUs.
Host Display ID and remove all guest PDUs
Host to Defaults
Guest to Defaults
Guest Management Interface (Reboot)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.