Browse FAQs

If the LCD User Interface in SRCE6KUXI model is hanged and not able to change any setting or see any text?

Published date: 03 June 2020

If the LCD User Interface in SRCE6KUXI model is hanged and not able to change any setting or see any text, then wait untill the back-light of LCD goes off (Approximately 2 minutes).
Press any button after the back light goes off. Now see LCD, if the same problem persists kindly contact the customer care.

Note: During this period do not press any button. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.