Browse FAQs

If the LCD display is showing error as by pass not available?

Published date: 03 June 2020

Check for the following conditions
  • ​Check whether the Jumper is connected on the rear panel, if not connected, connect the jumper and the fault will go off.
  • If the jumper is connected and the LCD is showing the error, then by-pass circuit breaker might have been tripped. Turn on the circuit breaker, the fault will go off.
If the issue still persist, contact the customer care.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.