Browse FAQs

Do the SRC5000UXI to 10000UXI models turn ON without battery, when the input power is available?

Published date: 21 May 2020

Yes.  The SRC5000UXI to 10000UXI models will turn ON if the battery is not connected when the input power is available.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.