Software / Firmware

Software / Firmware

PowerChute Network Shutdown v4.2 for Virtualization (32-bit systems only)
To know more about the supported systems, please visit this FAQ
Name File Type File Size (KB) File Date  
VMware ESX
PowerChute Network Shutdown v4.2 for VMware ESX Application 08/23/2016
   
VMware ESXi
PowerChute Network Shutdown v4.2 for VMware ESXi Application 08/23/2016
   
VMware Virtual Appliance
PowerChute Network Shutdown v4.2 VMware Virtual Appliance **Single / Redundant / Parallel UPS Configurations Only** Application 12/21/2017