AC Cooling equipment: ODC Ozone Depleting Chemicals
Published date:
18 July 2020
Issue:
This is a list of all Cooling units and the type of refrigerant that is used.
Product line:
All Cooling Units.
Environment:
All Product models, all serial numbers.
Cause:
Ozone Depleting Chemicals.
Resolution:
AC Cooling equipment: ODC Ozone Depleting Chemicals
There is a push from the EPA to move away from ODC’s used in refrigeration. You may be asked, especially from Canada sites, if our systems use ODC. Our current 2012 line of cooling equipment do not use ODC.However, some of our older systems do use R22 which is considered an ODC.
Which units use R22?
AFX, CCT, CM, FM, ACPA4000, and TC all use R22 which is an ODC
What other refrigerants do we use that are not ODC?
410a
ACPSCx, ACRD10x, ACSC10x, TDVAx
407c
ACRP10x, ACRD50x, ACPDX21-86
134a
RDU, OA,
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.