Browse FAQs



After upgrading firmware on my APC AP8XXX series Rack PDU, the input voltage reads 1V
Alternatively, downgrading the Rack PDU to rpdu2g v5.1.6 is a viable solution if none of the above can be ...
What are the basic troubleshooting steps for the G-Type Rack Power Filter; G5BLK?
APC G- Type Rack Power Filter ... Solution ... If it trips again, unplug one of the components plugged into the unit and reset the breaker. ... If the breaker is tripped again after trying this solution , contact APC Technical Support. ... Reduce the load by disconnecting one or more components from the back of the unit.
Why is my Web/SNMP (ap9606) or Network Management Card 1, 2 or 3 not recognizing my UPS or device?
... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... Device Type ... Single or three phase Smart-UPS, Galaxy 3500, Matrix UPS ... Single phase Smart-UPS (NMC3) ... Single Phase Symmetra UPS ... Rack Power Distribution Units Rack Power Distribution APP or rpdu ... Lastly, if the firmware upgrade does not resolve the issue, there may be a problem with the Network Management Card or the UPS SmartSlot.
Why are the red outlet LEDs always scrolling on Rack PDU models AP7855 or AP7867?
AP78XX Metered Rack PDU models, specifically ... Scenario 1 : ... Manually changing these values or resetting the unit to default settings should resolve this issue. ... (This will set to a non zero value) - sets the calibration value to known one . ... Connect a known load (must be greater than 5A) on L 1 Outlet 2. Then select the fourth menu "Calibrate the unit". ... If the user does not have the ability to connect a known load on L 1 outlet 2 then follow this second procedure.
Domain Name/DNS Hostname Parameters on the Network Management Card 1 and 2
... Network Management Card 1 and 2 ... Network Management Card 1 - AP9617, ... ... Network Management Card 1 include (but ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... ... Network Management Card 1 Behavior ... Network Management Card 1 (AP9617, ... resolves this issue. If you experience this problem, please update your Network Management Card 1 to an appropriate firmware version, if available.
Common Rack Automatic Transfer Switch Scenarios and Questions
... article discusses common Rack Automatic Transfer Switch ... Rack Automatic Transfer Switches ... All Rack ATS models listed ... As the Rack Automatic Transfer Switches ... ... BULLETIN - Upgrading Rack ATS Firmware ( ... ... for switching from one power source to ... ATS firmware v3.5.7 and higher aims to resolve this issue and will help prevent the ATS from tripping the upstream circuit breakers. ... Using the Rack ATS with a Generator
AP8XXX Rack PDU 2G "NMC CAN Bus Off" Error
... My AP8XXX series Rack PDU 2G ... Rack PDU ## ... Rack Power Distribution ... All AP8XXX Rack PDU 2G models ... The CAN bus on the Rack PDU products is represented to the user via In and Out Ports, noted in the below image. ... For units manufactured later than December, 2012, you may find a CAN bus terminator pre-installed in one of these ports. ... After a "CAN bus off" alarm has been resolved , the clearing event is not generated and the alarm remains in the active list.
What are the various generations of Smart-UPS Products?
... various generations of single phase Smart- ... Current Products: All units Rack / Tower convertible 1kva - 1 . 5kva 1 . 5kva - 3kva ... All units are Rack /Tower convertible ... can only use one at a time ... Rack / Tower or Rack / Stack convertible ... Rack / Tower or Rack / Stack convertible ... 5kva and larger include embedded Network Management Cards ... Legacy Products: 700va - 5kva ... 700va - 5kva ... Serial (DB-9 Serial Port) or USB Communications (You can only use one at a time) ... 420va - 1 . 5kva ... Tower and Rack /Tower convertible units
Video: How do I configure APC Network Management Card network settings?
... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... Network Management Card 1 : ... Network Management Card 1 (AP9617, ... Network Management Card 1 (such as ... AP78XX or AP79XX Rack PDU, Environmental ... ... Network Management Card 1 based devices are ... ... AP8XXX Next Gen Rack PDU (NMC2 ... ... device, select one of the available ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.