Technical FAQs

Ask a Question

NetBotz 750 | What parts come with the NetBotz 750?

Issue:
   Description of components that come with the NetBotz 750.

Product Line:
   NetBotz Rack Monitor 750

Environment:
   NetBotz 750 (all firmware versions)

Resolution:

Inventory


Item Quantity
1 NetBotz Rack Monitor 750 1
2 Wireless Coordinator & Router (NBWC100U) 1
3 Brackets for standard 19-in rack 2
4 Phillips flat head screws, M4 x 8 4
5 2-position terminal block plug 2
6 3-position terminal block plug 2
7 9-position terminal block plug 1
8 tie wraps, 203 mm (8 in) 2
9 IEC-320-C13 to IEC-320-C14 power cord, 1.8 m (6 ft) 1
10 NEMA 5-15P to IEC-320-C13 power cord, 1.8 m (6 ft) 1
11 USB-A to Micro USB-B cable, 2 m (6 ft) 1
12 A-Link Terminator 1

Not Shown:
Description Quantity
Temperature/Humidity Sensor (AP9335TH) 1
Wireless temperature sensor (NBWS100T) 1
Basement mount hardware kit (0M-814726) 1
Was this helpful?
What can we do to improve the information ?